Part Number: LMK04828
Other Parts Discussed in Thread: LMK04832,
In this link (https://www.ti.com/clocks-timing/jitter-cleaners-synchronizers/products.html#p2192=JESD204B&p1811=32;98.8125&sort=p1451;asc), there are several different parts that support JESD204 clock generation. I am looking for some marketing slides that can give a more detailed comparison than just the columns in that table can provide.
For general context, I am looking to evaluate different clock generators for a single (not multiple chip) RFSoC application. The applications needs deterministic latency, and tile synchronization and the RFSoC requires SYSREF signals for that purpose leading me to JESD204 parts. Our clock source will be a very accurate 10MHz OXCO, and we need to generate frequencies from 200MHz-600MHz (being able to generate up to 3GHz would be nice). 7 data clocks are required and then 2 SYSREFs attached to two of those clocks (9 total outputs). Other than that, the number one priority is phase noise performance across all offset frequencies (i.e. 1Hz to 20MHz) in that 400MHz +/- 200MHz output range.
Any marketing material or suggestions would be appreciated
Thanks,
Nino