This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571: Which Power pin is dedicated to the RFOUTTX/RX driver?

Part Number: LMX2571


Hi Team,

Please advise me on my question bellow:

Q1. There are total seven pins for the power. 

    can you let me know which power pin is dedicated to the output driver for the RFOUT TX/RX.

I  am experiencing a loss of lock trouble using LMH2571 in Push-Pull output mode.

I programmed the output power at maximum (31h), the device showed loss of lock.

When I reduced the output power as low as (03h), the device kept lock.

I suspect that large output power interferes the PLL resulting loss of lock.

In doer to isolate the output driver from the lest of circuit inside the device, I want to know

which power pin is dedicated or connected to the driver.

Mita  

  • Hi Mita,

    Could you provide your software configuration? What are the input and output frequencies?

  • Noel-san,

    Thank you for your feedback.

    Please find code bellows: It is one of an example of my configuration.

      Input:  56.64 MHz

      PDF:  99.12 MHz

      VCO: 5008.952687931 MHz

      Output:  500.8952687931 MHz

    BTW:  Can you give me the answer to my question?

    [SETUP]
    ADDRESS=888
    CLOCK=8
    DATA=4
    LE=2
    PART=LMX2571
    IFACE=SPI
    ADDRESS_I2C=0x0
    
    [PINS]
    PINNAME00=TrCtl
    LOCATION00=7
    PINVALUE00=True
    PINNAME01=CE
    LOCATION01=0
    PINVALUE01=True
    
    [MODES]
    NAME00=R60
    VALUE00=3973120
    NAME01=R58
    VALUE01=3836928
    NAME02=R53
    VALUE02=3504134
    NAME03=R47
    VALUE03=3096576
    NAME04=R46
    VALUE04=3014681
    NAME05=R42
    VALUE05=2753040
    NAME06=R41
    VALUE06=2689048
    NAME07=R40
    VALUE07=2627612
    NAME08=R39
    VALUE08=2560507
    NAME09=R35
    VALUE09=2296967
    NAME10=R34
    VALUE10=2281473
    NAME11=R33
    VALUE11=2162688
    NAME12=R32
    VALUE12=2097152
    NAME13=R31
    VALUE13=2031616
    NAME14=R30
    VALUE14=1966080
    NAME15=R29
    VALUE15=1900544
    NAME16=R28
    VALUE16=1835008
    NAME17=R27
    VALUE17=1769472
    NAME18=R26
    VALUE18=1703936
    NAME19=R25
    VALUE19=1638400
    NAME20=R24
    VALUE20=1572895
    NAME21=R23
    VALUE21=1515332
    NAME22=R22
    VALUE22=1475975
    NAME23=R21
    VALUE23=1376516
    NAME24=R20
    VALUE24=1323033
    NAME25=R19
    VALUE25=1245184
    NAME26=R18
    VALUE26=1204630
    NAME27=R17
    VALUE27=1114180
    NAME28=R16
    VALUE28=1048576
    NAME29=R15
    VALUE29=983040
    NAME30=R14
    VALUE30=917504
    NAME31=R13
    VALUE31=851968
    NAME32=R12
    VALUE32=786432
    NAME33=R11
    VALUE33=720896
    NAME34=R10
    VALUE34=655360
    NAME35=R9
    VALUE35=589824
    NAME36=R8
    VALUE36=524319
    NAME37=R7
    VALUE37=466692
    NAME38=R6
    VALUE38=427399
    NAME39=R5
    VALUE39=327940
    NAME40=R4
    VALUE40=266262
    NAME41=R3
    VALUE41=196608
    NAME42=R2
    VALUE42=149797
    NAME43=R1
    VALUE43=65618
    NAME44=R0
    VALUE44=579
    
    [FLEX]
    Fosc_F1_FREQ=57.6
    Fosc_F2_FREQ=56.64
    Fosc_FREQ=56.64
    Fout_F1_FREQ=450.000000515
    Fout_F2_FREQ=500.8952687931
    Fout_FREQ=500.8952687931
    Fpd_F1_FREQ=100.8
    Fpd_F2_FREQ=99.12
    Fpd_FREQ=99.12
    Fvco_F1_FREQ=4500.0000051498
    Fvco_F2_FREQ=5008.952687931
    Fvco_FREQ=5008.952687931
    TrCtl_Pin=1
    btn_SimplifyFraction=Simplify Fraction
    btn_SpurBGone=Spur-b-Gone
    flexCHDIV1=5
    flexCHDIV2=1
    flexCurrent=53.7
    flexEXTVCO_CHDIV=0
    flexExtVCO_FREQ=480
    flexFRAC_ORDER=3
    flexIntVCO_FREQ=5008.952687931
    flexKpd=2.5
    flexKvco=62.26858099241
    flexMULT=7
    flexOUTBUF_RX_EN=1
    flexOUTBUF_RX_PWR=31
    flexOUTBUF_TX_EN=0
    flexOUTBUF_TX_PWR=31
    flexOutputDivide=10
    flexPFD_DELAY=4
    flexPLL_DEN=0
    flexPLL_N=25
    flexPLL_NUM=4481430
    flexPLL_N_PRE=0
    flexPLL_R=1
    flexPLL_R_PRE=4
    

    Mita

  • Hi Mita-san,

    Pin15 is the power supply pin for the output buffer.

    Your software configuration is basically ok, except that MULT_WAIT should be increased to 1132 in order to meet the 20µs requirement.

    When you say loss lock, did you simply mean MUXout is LOW? Could you check the Vtune voltage (pin 25) and also the output signal with a spectrum analyzer? You'd better make OUTBUF_AUTOMUTE = 0 so that the output buffer will not mute even if it is unlock. 

  • Noel-san,

    Thank you for the answer as well as your advise.

    I will try it with MULT_WAIT=1132.

    Mita

  • Noel san

    Thank you for your LMX2571's support and cooperation always!
    We work on it with Mita san.

    We tried it with MULT_WAIT=1152(@OSCin=57.6MHz).
    However, it didn't solve.
    Furthermore, we configured Loop filter setting to gain enough phase margin.

    When we reduced the output power(OUTBUF_RX_POW) as low as (03h~04h), the device kept lock.

    We would like to confirm that we suspect that large output power interferes the PLL resulting loss of lock again.
    (For example, it affects to internal power line via output amp stage of large power level.)

    Especially, we also would like to confirm whether it depends on board layout.


    Kind regards,

    Hirotaka Matsumoto

  • Hi Matsumoto-san,

    03h-04h are very low output power setting, I have never encountered this problem before.

    How many LMX2571 has this problem? If every LMX2571 has this problem, then I believe it may be an application issue, like layout problem or wrong schematic or wrong component values. 

    If only one LMX2571 has this problem, can they try if making the output frequency = 495.6 MHz (this is an integer channel with NUM=0) can resolve the problem? 

  • Noel san

    Thank you for your reply!

    How many LMX2571 has this problem?
    ->20 devices (20/170), therefore we think we believe it may be an application issue, like layout problem or wrong schematic or wrong component values also.   
       We will check the board layout and circuit.

    Kind regards,

    Hirotaka Matsumoto