This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05028: LMK05028

Part Number: LMK05028


i want to use one of the inputs of LMK05028

my input signal is 100MHZ LVCMOS. I saw on the elec. characteristics (p10 on datasheet) that the input freq of LVCMOS input is between 1-250Mhz,

but on the pin function explanation (p.5) it is written that LVCMOS input mode is recommended for input freq from 5M to 1 hz...

it is possible to connect LVCMOS 100MHZ input to the LMK05028 input pin?