Part Number: LMX2594
Hello,
We have made a custom board with the LMX2594 with the schematic being almost exactly the same as the EVM (the 100MHz reference being VC-708-EDE-FNXN-100M000000)
3.3V to the oscillator and the LMX2594 are being generated on-board using the LDO AP7361C-FGE-7.
There are two issues that we noticed:
1) The frequency in not 100% locked. It keeps shifting by a few hundred Hz.
2) As we change the supply to the LDO (from 4V to 5.5V) the close in spurious keep changing frequency and levels (do not know if they are the PFD spurs).
We are using the TI GUI to program our board (and are using the default settings)
Following is a single capture

Looking forward to your inputs in fixing the problem. Thank you for your help in advance,
Regards,