Part Number: LMK04832
Hello team,
The LMK04832’s data sheet only describes typical values for phase noise parameters, but I need the worst ones. Please share with me if the Max values are available. If not, average and stddev ones from the characterization data are OK for me.
In addition, if there are test result data in several temperatures within the test environment of datasheet figure2 and 3? (2500MHz and 3200Hz)
Best regards,
Ryotaro Fukui