Part Number: LMK03328
I'm developing some code to program device settings into EEPROM page 0 on the LMK03328.
Writing the registers is successful (the required output frequencies appear at the two outputs we are using). However the setting don't appear to be saved in EEPROM, despite the EEPROM write count being incremented.
We are leaving much greater than the recommended 230ms for transfer of SRAM data to the EEPROM, but how long does a transfer of registers to SRAM take? We are possibly not waiting lng enough for the register settings to be transferred to the SRAM before starting the write to EEPROM.
Can R137 be read during this time to check for completion of the transfer to SRAM (or will this abort the process)?