This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: Output behavior when no input

Part Number: LMK04832

Hello team,

I have a questions about LMK04832.

I consider to operate LMK04832 in distribution mode.

And, I consider inputting LVPECL diff signal of buffer IC output to CLKin1(pin34, 35) of LMK04832 and datasheet 9.1.2.1 of LMK04832 says connection should be AC coupled because it is internally biased.

  1. Is there a possibility that LMK04832 will output oscillation when buffer IC is OFF and no signal is input to LMK04832?
  2. If it can be happened, please let me know a way to avoid the behavior?

Best regards,