Part Number: TPL5010
Hello
I'd like to inquire about the watchdog chip tpl5010. My client has a project that using this watchdog chip. The timing resistance is selected to wake up once every 6 minutes, but we can't wait for 6 minutes for factory test. We do a switching resistance to complete factory test. When measuring the watchdog function, we switch to the resistance of 6 seconds, but the actual test shows that the function is not functional, Therefore, I would like to ask whether the pin of the chip timing resistance only reads the resistance of the pin just after power on to determine the wake-up time. If the chip is powered on with a resistance of 6 minutes and then switched to 6 seconds, will the chip read the timing resistance again and switch the timing time?