Part Number: SA555
Other Parts Discussed in Thread: TLC555
Hello guys,
One of my customers is considering using SA555 for their new products.
They want to achieve very long timer using SA555 with Figure 9 Circuit for Monostable Operation on page 10 of SA555 datasheet (Ver .SLFS022I).
For the timer, they have several questions as the follows.
Could you please give me your reply for them?
Q1. What is VCC range can Figure 11 Output Pulse Duration vs Capacitance graph on page 10 be applied for?
Q2. I can see "Ra=10Mohm" in Figure 11 graph.
Can 10Mohm be used for Ra when VCC is 5V in the worst case?
I think RA should be less than 3.2Mohm when VCC is 5V because the capacitor placed between THRES pin and GND can not charged to the THRES voltage
through Ra in case of 4.2V THRES voltage level (Max value) and 250nA THRES current (Max value).
Q3. What is the maximum value of the capacitor placed between THRES pin and GND?
Is there not limited? Or is it less than 100us which is the maximum value of Figure 11 graph to protect discharge transistor connected to DISCH(No.7)?
Your reply would be much appreciated.
Best regards,
Kazuya.