Part Number: LMX2594EVM
Other Parts Discussed in Thread: USB2ANY, LMX2594, LMX2592,
I am operating system that contains all three of the above components. As of yesterday they were all operating as expected, however this morning they no longer output a signal.
All three devices are operated through the TICS Pro and interface with my computer through the USB to any devices.
I have tested power cycling and reloading the registers through TICS Pro, however there is still no output form any of them. In addition when I use TICS Pro to read back the raw registers they all come back as empty leading me to believe that the registers are not loading properly when I submit them through TICS Pro.
The only commonality between the devices, other than the fact they are all connected to the same computer, is that they share a power line.