Other Parts Discussed in Thread: DS100MB203, DS64MB201, DS42MB200, DS40MB200
Hello
I have 2 lanes (each lane is a differential pair) which I need to duplicate each of them. so each lane will have 2 fully independent outputs.
My application is VBO-HS video signals which can be from 0.6 gbps to 4 gbps. so I need very low skew especially between lanes. no modification or termination required, just duplicating the signal. think of it as exactly the same as HDMI and DP fanout or splitter ICs.
I saw TI part DS100MB203 which seems suitable but it is very pricey at ~ 15$ or so, I need it to be cheaper if exist.
I have microchip SY58606UMG part which is suitable but only one lane per IC which makes it a bit harder.
for your kind help.
thanks