Part Number: LMK04828
Hello,
In The Data Sheet the SPI pins have this note " Nominal 160-kΩ pulldown"
What does it means ?
Do the Pulldown Resistor is built in or external 160Kohm is needed ?
Thanks
Ronen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ronen,
The 160kΩ nominal pulldown resistance is internal to the device on each SPI input pin.
Regards,
Derek Payne