Other Parts Discussed in Thread: TLC555
Dear Team,
Out customer need RC timer solution: similar with 555 oscillator.
Vcc 12V
Frequency: 50HZ~60HZ
operating temp : -40~+105
Please advise. Thanks.
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jimmy,
The TLC555Q1 can operate from -40 to 125C.
I have put together a simulation using the TLC555 running at 12V with approximately 50Hz. The simulation is attached at the bottom of this post. The RC values can be modified to the desired values and achieve the appropriate frequency using the equations below.