Other Parts Discussed in Thread: CDCE62002
Hi,
Not sure if this has been answered in a previous post by another person.
I have scanned the latest (March 2011) CDCE62002 data sheet and i do not believe the answer is there.
For a READ command to the CDCE62002 does the IC send all 32 bits or just the 28 data bits ?
The SPI_MISO shows Bit0, Bit1, Bit2 sent etc., so are these SPI BITS such that the 28 Data bits are sent after SPI BIT3 ??.
Thanks and regards,
Richard.