Part Number: CDCLVD2102
I can't find any information on having active input signals (LVDS with 1.6V CM) on an un-powered device. Is there any information on this? Is this likely to damage the device or provide a leakage path back to the power supply of the device? My use case would have the board powered off but attached to a system that is powered on and driving the inputs to the CDCLVD2102.
Thanks,
Doug