This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03806: SYNC pin control method

Guru 12825 points

Part Number: LMK03806
Other Parts Discussed in Thread: LMK04806

Hello,

My customer wnats to use the sync pin of the LMK03806 to synchronize the phase of all the clock outputs.

For this, please explain in detail how to control the sync pin.

When SYNC_POL_INV is set to 1, should the sync pin input be toggled from High to Low once after the output clock has stabilized? After this, if the sync pin input is kept low, will the sync be maintained?

When the sync pin input is connected as pull-down, is it possible to synchronize even if SYNC_POL_INV is controlled from low to high?

Thank you.

JH