Part Number: CDCM6208
Hi team,
When inputting single-end clock to secondary reference input, how should I terminate SEC_REFN?
Should it be pulled down with 1kOhm resistor?
Also, should PRI_REFN be pulled down with 1kOhm as well?
Regards,
Itoh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCM6208
Hi team,
When inputting single-end clock to secondary reference input, how should I terminate SEC_REFN?
Should it be pulled down with 1kOhm resistor?
Also, should PRI_REFN be pulled down with 1kOhm as well?
Regards,
Itoh
Hi Timothy-san,
In the above thread, it is mentioned that unused pin can be pulled up/down with 1kOhm resistor.
Is it different if the single-end clock is used?
Regards,
Itoh
Hello Itoh-san,
You are correct. I found in another thread the advice to leave open. Let me double check. Certainly with the pull-up/pull-down you cannot go wrong as you can always leave the components un-populated.
73,
Timothy
Hello Itoh-san,
It is not required to place any other components with driving CDCM6208 single ended. The only requirements are the Vih/Vil levels listed in the datasheet.
When unused and the input buffer is powered down, there is no need for any biasing, the inputs can be left floating.
If the input is used, but no clock present, the inputs do have hysteresis to prevent chattering as listed in the datasheet. Only if you have excessive noise what would exceed the hysteresis level would the addition of pull-up/pull-down on opposite pins be of any use. You would want to put the pull-down on the pin which is biased at the lower level - which I'm not sure off-hand which pin that is.
73,
Timothy