Part Number: TLC555
Hi Team,
I am looking at the TI TLC555IDR for use in an existing design with an immediate need for 10K pieces. I see TI factory stock listed at >250K so it would be great if this part can meet our application requirements.
I am comparing the TLC555I to the ST TS555IDTR that is currently used on the design. In many ways the TLC555I is a better IC but there are a couple of specifications that I do not see in the datasheet and would like to confirm that they good for this application.
Would it be possible for you to share the following specifications?
- Timing shift over temperature coefficient. In other 555 datasheets this is given in units of PPM/oC.
- Astable timer accuracy at Vdd=12V and / or Vdd=15V. The datasheet only list accuracy at Vdd=5V.
Regards,
RJ