I am using the LMX2595 in Full Assist mode, with all the relevant force bits set high and everything
I've noticed that the MUXOUT signal only goes high for Lock Detect when the FCAL_EN bit is asserted, is this normal and necessary for the lock detect to work in Full Assist mode?
EDIT: Conversely, I can not seem to get the lock detect bit to go high when it is in full assist mode without that FCAL_EN bit asserted.