Other Parts Discussed in Thread: LMX2615EVM-CVAL
Hello,
The LMX2615-SP wideband Synthesizer operates on a very wide band ( from 40 MHz to 15 GHz).
In my application, I'am operating at one single fixed frequency ( around 5 GHz).
On eval board LMX2615EVM-CVAL, at 5.0 GHz, with default matching circuits (red box), on channel A and B, the measured output power is around +3.5- to+4.0 dBm.
I would like to optimize the matching circuit to increase the output power for my fixed operating frequency.application.
Do you have an electrical model for the impedance seen at pins 36 and 37 (red arrow) ?
With such information, with ADS, I could modify the values for L1, C5, C6 and C7 to get more power.
Thanks