Part Number: LMK04806
Other Parts Discussed in Thread: CODELOADER
Hi team,
I‘m remote supporting a semiconductor tester project. Customer would like to input a 100MHz OSC to PLL2 through OSCin, powerdown PLL1, and set internal VCO to 2.4G, then divide to 12 channels of clean 100MHz CLKout. They have problem that the HEX configuration attached below doesn't achieve what they want. I can't take an onsite support, but just paper review. Could you pls take a look at the configuration? What I've seen is they should set the phase detector polarity for PLL2 positive.
Thanks.
R0 (INIT) 0x80160140 R0 0x00140300 R1 0x00140301 R2 0x00140302 R3 0x00140303 R4 0x00140304 R5 0x00140305 R6 0x11110006 R7 0x11110007 R8 0x11110008 R9 0x55555549 R10 0x9102410A R11 0x3000100B R12 0x0B0C00AC R13 0x1302080D R14 0x0200000E R15 0x8000800F R16 0xC1550410 R24 0x00000058 R25 0x02C9C419 R26 0xAFA8001A R27 0x10001E1B R28 0x00201E1C R29 0x0180019D R30 0x0200019E R31 0x001F001F