Other Parts Discussed in Thread: LMX2582,
Hello,414.25MHz_RX_Local_150kHzoff_spurious_20211119.zip
Our customer is verifying performance of LMX2571EVM for 470MHz TX/RX.
Their finding is 100KHz and 150KHz off spurious issue.
There is combination condition, TCXO 16.8MHz with PLL output 414.25MHz is one of significant tough condition. We have observed 100kHz -39dBc and 150kHz -53dBc.
In the case of 100KHz spurious, if use setting of Multiplier is x1 and Post-R is 1/, then spurious level is improved to below noise floor.
About 150KHz spurious, it is large level as -53dBc when Fractional setting is 1st order. But change it to 4th order, spurious is disappeared as attached file.
What is root cause of phenomena? How can we optimize registers setting?
Regards,
Mochizuki