This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCVF2505: pin to pin with ICS9112AM

Part Number: CDCVF2505

Hi Sir,

May I confirm if we can use CDCVF2505DR to drop replacement ICS9112AM? Or there is other better drop replacement recommendation?

If we can use CDCVF2505DR, any difference should be care? 

ICS9112AM datasheet:

https://www.renesas.com/us/en/document/dst/9112a-16-datasheet

Thank you.

Regards,

Allen

  • Hi Allen,

    The CDCVF2505 can be used as a replacement for the ICS9112AM. Below is a table showing the differences.

    Our device has a larger frequency and temperature range, as well as a lower output skew, propagation delay and cycle to cycle jitter. 

    CDCVF2505 ICS9112AM
    Max supply voltage [V] 4.3 7
    Frequency range [MHz] 24 to 200 25 to 133
    Max output skew [ps] 150 250
    Max tRISE/ tFALL [ns] 2 1.5
    Max propagation delay [ps] 150 350
    Max cycle-to-cycle jitter [ps] 150 200
    Operating temp [°C] -40 to 85 0 to 70

    Regards,

    Jennifer