Part Number: LMX2592
Hi team,
There are three questions. Could you support this?
1. We can see fOUT = 606.25 MHz on the figure 23 of the datasheet. Are there any information of the 2nd, 3rd, 4th and 5th harmonic distortion for fOUT?
If you don't have any data, are there any ways to estimate the distortion?
2. On the figure 23, we can see the divider, 1/8. Is it possible to change the number of denominator, 8 to other number? Especially, they want to change it to not integer, but decimal like 1.2 and so on. Is this possible?

3. From what frequency the VCO doubler start to be activated?
4. Their output range is 3GHz~9GHz. And they want to make the harmonic level -40~-50dBc. Do you think it's possible to achieve the distortion level?
They guess the distortion level of the fundamental frequency for the doubler can be high.
5. If LMX2592 can't meet their requirement( output range is 3GHz~9GHz, the harmonic level -40~-50dBc), are there any recommendation else?
Regards,
Noriyuki Takahashi