This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: automatic ramp bandwidth

Part Number: LMX2594

Hello,

The output is divided by 24 and tested its output frequency with spectrometer.Both in Automatic Ramping mode, the initial frequency is 11300 MHz. Set the final frequency to 11470 (left figure) and 11500 (right figure).

It can be seen that  exceed 11470Mhz are no longer output (test bandwidth is 50MHz). Therefore, when set to 11500MHz, the output frequency is 11470MHz.

So we would like to confirm the automatic ramp bandwidth.

Best regards

Kailyn