Part Number: LMX2582
Hi team,

Why will inductor pullup increase output power at the resonance frequency?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joanne,
When the output is connected to a 50Ω load, if the pull-up is 50Ω resistor, the output will see a 50//50 = 25Ω load. If the pull up is an inductor, it will appear as high impedance so the load is still 50Ω. Voltage swing will be higher with a higher impedance load.