This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214: Application for the TDA4 PCIE 100MHz and Register set

Part Number: CDCE6214

Hi Ti:

We want used CDCE6214 in pin mode. Is the CDCE6214 can content application for the TDA4 PCIE 100MHz in defult? Is it must be according TDA4 REF design to series 33ohm and 50ohm to gnd?

Is it must be set to 1 for Register R79 bit9? And Is it must be set to 1 for Register 0x39/0x3f/0x44/0x49 bit12? When we used VDDO12/VDDO34 be 1.8V.

Thanks!!

  • Hello,

    Please find the default configurations for EEPROM page 0 and page 1 attached and see if the default configurations work for you. If it does, then simply configure the HW_SW_CTRL pin to select the right EEPROM page. You can review these configurations in Ticspro by doing: File -> import hex registers. By default it's using 25MHz XTAL on SECREF.

    R85	0x00550000
    R84	0x00540000
    R83	0x0053FF00
    R82	0x005201C0
    R81	0x00510004
    R80	0x00500008
    R79	0x004F0008
    R78	0x004E0000
    R77	0x004D0002
    R76	0x004C0188
    R75	0x004B0008
    R74	0x004AA181
    R73	0x00492000
    R72	0x00480006
    R71	0x00470406
    R70	0x00460008
    R69	0x0045A181
    R68	0x00442000
    R67	0x00430006
    R66	0x00420006
    R65	0x00414008
    R64	0x0040A181
    R63	0x003F2000
    R62	0x003E0006
    R61	0x003D0000
    R60	0x003C0008
    R59	0x003B0008
    R58	0x003A502C
    R57	0x00394000
    R56	0x00380006
    R55	0x0037001E
    R54	0x00363400
    R53	0x00350069
    R52	0x00345000
    R51	0x003340C0
    R50	0x003201C0
    R49	0x00310013
    R48	0x00301A05
    R47	0x002F0280
    R46	0x002E0000
    R45	0x002D4F80
    R44	0x002C0318
    R43	0x002B0051
    R42	0x002A0002
    R41	0x00290000
    R40	0x00280000
    R39	0x00270000
    R38	0x00260000
    R37	0x00250000
    R36	0x00240000
    R35	0x00230028
    R34	0x00220000
    R33	0x00210000
    R32	0x00200000
    R31	0x001F0000
    R30	0x001E0030
    R29	0x001D0000
    R28	0x001C0000
    R27	0x001B0004
    R26	0x001A0000
    R25	0x00190400
    R24	0x0018091C
    R23	0x00172406
    R22	0x001606A2
    R21	0x00150590
    R20	0x00140000
    R19	0x00130000
    R18	0x00120000
    R17	0x001126C4
    R16	0x0010921F
    R15	0x000FA037
    R14	0x000E0000
    R13	0x000D0000
    R12	0x000C0000
    R11	0x000B0000
    R10	0x000AA777
    R9	0x00097BFA
    R8	0x00080001
    R7	0x00070C2D
    R6	0x00060E6C
    R5	0x00050008
    R4	0x00040000
    R3	0x00030200
    R2	0x00020000
    R1	0x00017654
    R0	0x00000001
    
     

    R85	0x00550000
    R84	0x00540000
    R83	0x0053FF00
    R82	0x005201C0
    R81	0x00510004
    R80	0x00500008
    R79	0x004F0008
    R78	0x004E0000
    R77	0x004D0002
    R76	0x004C0188
    R75	0x004B8008
    R74	0x004AA181
    R73	0x00490000
    R72	0x00480006
    R71	0x00470406
    R70	0x00460808
    R69	0x0045A181
    R68	0x00440000
    R67	0x00430006
    R66	0x00420006
    R65	0x00414808
    R64	0x0040A181
    R63	0x003F0000
    R62	0x003E0006
    R61	0x003D0000
    R60	0x003C6028
    R59	0x003B8008
    R58	0x003A502C
    R57	0x00390000
    R56	0x00380006
    R55	0x0037001E
    R54	0x00363400
    R53	0x00350069
    R52	0x00345000
    R51	0x003340C0
    R50	0x003201C0
    R49	0x00310013
    R48	0x00301A05
    R47	0x002F0280
    R46	0x002E0000
    R45	0x002D4F80
    R44	0x002C0318
    R43	0x002B0051
    R42	0x002A0002
    R41	0x00290000
    R40	0x00280000
    R39	0x00270000
    R38	0x00260000
    R37	0x00250000
    R36	0x00240000
    R35	0x00230028
    R34	0x00220000
    R33	0x00210000
    R32	0x00200000
    R31	0x001F0000
    R30	0x001E0030
    R29	0x001D0000
    R28	0x001C0000
    R27	0x001B0004
    R26	0x001A0000
    R25	0x00190400
    R24	0x0018091C
    R23	0x00172406
    R22	0x001606A2
    R21	0x00150513
    R20	0x00140000
    R19	0x00130000
    R18	0x00120000
    R17	0x001126C4
    R16	0x0010921F
    R15	0x000FA037
    R14	0x000E0000
    R13	0x000D0000
    R12	0x000C7002
    R11	0x000B003F
    R10	0x000AA777
    R9	0x0009A777
    R8	0x00080001
    R7	0x00070C0D
    R6	0x00060E6C
    R5	0x00050008
    R4	0x00040000
    R3	0x00030200
    R2	0x00020000
    R1	0x00017652
    R0	0x00002000
    

    Regards,
    Hao