Hello,
My customer is evaluating LMK04826B on their PCB.
They are facing an issue about digital delay.
Their configurations are as attached .tcs file.
Register Setting.tcs
After toggling SYNC_POL bit, CLKoutX+/- (X=8, 9, 10 and 11) polarity get the same and differential output magnitude become almost zero as follows.
After that, by writing SDCLKoutY_FMT bits Powerdown and then LVDS again, CLKoutX+/- (X=8, 9, 10 and 11) polarity get back to normal and CLKoutX+/- (X=8, 9, 10 and 11) start working well as follows.
This issue is observed when output frequency is 245.7MHz, but not observed when output frequency is 122.88MHz
Do TI experts have any suggestions or advises about this issue?
Best regards,
K.Hirano