Part Number: CDCEL913
Hi, support team
My customer has the questions as follow:
I am using CDCEL913.
I can output integer frequency, such as 33MHz
However, once there are decimals, such as 32.768 MHz, the output is incorrect.
For example, I set 32.768MHz, but my oscilloscope measures 4MHz.
This is my register configuration, which is obtained through Pro-Clock software:
Bit ==> 76543210 Byte 00 - 00000001 Byte 01 - 00000000 Byte 02 - 10110100 Byte 03 - 00000111 Byte 04 - 00000010 Byte 05 - 01010000 Byte 06 - 01000000 Byte 07 - 00000000 Byte 08 - 00000000 Byte 09 - 00000000 Byte 10 - 00000000 Byte 11 - 00000000 Byte 12 - 00000000 Byte 13 - 00000000 Byte 14 - 00000000 Byte 15 - 00000000 Byte 16 - 00000000 Byte 17 - 00000000 Byte 18 - 00000000 Byte 19 - 00000000 Byte 20 - 00001101 Byte 21 - 00000010 Byte 22 - 00000000 Byte 23 - 00000000 Byte 24 - 11100000 Byte 25 - 00000010 Byte 26 - 10100011 Byte 27 - 10000011 Byte 28 - 11100000 Byte 29 - 00000010 Byte 30 - 10100011 Byte 31 - 10000000

And this is my C configuration code. I can make sure that the register is written in, because the output integer frequency is OK.
#include "cdce913.h"
#include "iic.h"
#include <stdbool.h>
#include "math.h"
/************************************************
* File Name: @@@.c
* Author:xykj
* Date:2019.11.29
* function:cdce913
*************************************************/
void CDCE913_Init_invar(void)
{
cdce913_I2C_WriteByte(0x02, 0x34); //
cdce913_I2C_WriteByte(0x03, 0x1A); //y1·ÖƵ
cdce913_I2C_WriteByte(0x04, 0x02); //s0=0,s0=1¾ùѡͨ
cdce913_I2C_WriteByte(0x05, 0x50); //10PF ¾§ÕñµçÈÝ
cdce913_I2C_WriteByte(0x06, 0x40);
cdce913_I2C_WriteByte(0x12, 0X00); //SSC1_1[5:3] AND SSC1_0[2:0] XXX XXX
cdce913_I2C_WriteByte(0x13, 0X00); //s0=0,Ñ¡Ôñfvco1 s0=1,Ñ¡ÔñFVCO_0
cdce913_I2C_WriteByte(0x14, 0x6D); //ʹÓÃPLL1£¬Y2ʹÓÃpdiv2£¬y3ʹÓÃpdiv3 0110 1101 (6D)
cdce913_I2C_WriteByte(0x15, 0X02); //S0=0,S0=1´ò¿ª
cdce913_I2C_WriteByte(0x16, 0X7D); //y2·ÖƵ 0Ϊ¹Ø
cdce913_I2C_WriteByte(0x17, 0X00); //y3·ÖƵ 0Ϊ¹Ø
cdce913_I2C_WriteByte(0x18, 0X7C); //N
cdce913_I2C_WriteByte(0x19, 0XE2); //N
cdce913_I2C_WriteByte(0x1A, 0XC2); //R
cdce913_I2C_WriteByte(0x1B, 0X68); //Q
cdce913_I2C_WriteByte(0x1C, 0X7C); //N
cdce913_I2C_WriteByte(0x1D, 0XE2); //N
cdce913_I2C_WriteByte(0x1E, 0XC2); //R
cdce913_I2C_WriteByte(0x1F, 0X68); //Q
}
//void CDCE913_Init_invar(void)
//{
// cdce913_I2C_WriteByte(0x02, 0xB4); //
// cdce913_I2C_WriteByte(0x03, 0x7E); //y1·ÖƵ
// cdce913_I2C_WriteByte(0x04, 0x02); //s0=0,s0=1¾ùѡͨ
// cdce913_I2C_WriteByte(0x05, 0x50); //10PF ¾§ÕñµçÈÝ
// cdce913_I2C_WriteByte(0x06, 0x40);
//
// cdce913_I2C_WriteByte(0x12, 0X00); //SSC1_1[5:3] AND SSC1_0[2:0] XXX XXX
// cdce913_I2C_WriteByte(0x13, 0X00); //s0=0,Ñ¡Ôñfvco1 s0=1,Ñ¡ÔñFVCO_0
// cdce913_I2C_WriteByte(0x14, 0x2D); //ʹÓÃPLL1£¬Y2ʹÓÃpdiv2£¬y3ʹÓÃpdiv3 0110 1101 (6D)
// cdce913_I2C_WriteByte(0x15, 0X02); //S0=0,S0=1´ò¿ª
//
// cdce913_I2C_WriteByte(0x16, 0X00); //y2·ÖƵ 0Ϊ¹Ø
// cdce913_I2C_WriteByte(0x17, 0X00); //y3·ÖƵ 0Ϊ¹Ø
// cdce913_I2C_WriteByte(0x18, 0X6A); //N
// cdce913_I2C_WriteByte(0x19, 0X59); //N
// cdce913_I2C_WriteByte(0x1A, 0X82); //R
// cdce913_I2C_WriteByte(0x1B, 0X89); //Q
// cdce913_I2C_WriteByte(0x1C, 0X6A); //N
// cdce913_I2C_WriteByte(0x1D, 0X59); //N
// cdce913_I2C_WriteByte(0x1E, 0X82); //R
// cdce913_I2C_WriteByte(0x1F, 0X88); //Q
//
//
//}
#define CLK_IN 26
void CDCE_Init_set(float f_out)
{
uint8_t read_back;
uint8_t i = 0;
uint32_t M, N, Q, R;
float Pdiv;
uint8_t reg18, reg19, reg1A, reg1B;
int32_t P;
float f_vco = f_out;
bool result = false;
uint8_t f_range;
while (f_vco < 80)
{
i++;
f_vco = f_out * i;
}
while (f_vco < 231)
{
for (N = 4095; N > 0; N--)
{
for (M = 511; M > 0; M--)
{
if ((N * CLK_IN / M) == f_vco)
{
{
result = true;
break;
}
}
}
if (result)
{
break;
}
}
if (result)
{
break;
}
else
{
i++;
f_vco = f_out * i;
}
}
P = 4 - (int)((log((double)N / (double)M))/log(2));
if (P < 0)
{
P = 0;
}
Q = (int)((double)N * pow(2, (double)P) / (double)M);
R = (double)N * pow(2, (double)P) - M * Q;
if (f_vco < 125)
{
f_range = 0;
}
else if ((f_vco >= 125) && (f_vco < 150))
{
f_range = 1;
}
else if ((f_vco >= 150) && (f_vco < 175))
{
f_range = 2;
}
else
{
f_range = 3;
}
Pdiv = f_vco/ f_out;
cdce913_I2C_WriteByte(0x02, 0xB4);
cdce913_I2C_WriteByte(0x03, (uint8_t)Pdiv);
cdce913_I2C_WriteByte(0x04, 0x02);
cdce913_I2C_WriteByte(0x05, 0x50);
cdce913_I2C_WriteByte(0x06, 0x40);
cdce913_I2C_WriteByte(0x12, 0x00);
cdce913_I2C_WriteByte(0x13, 0x00);
cdce913_I2C_WriteByte(0x14, 0x6D); //Y2,Y3¿ª¹Ø¿ØÖÆ£¬y1²»ÊǸÃÒý½Å¿ØÖÆ£¬¹Ì¶¨ÓÐY1
cdce913_I2C_WriteByte(0x15, 0x02);
cdce913_I2C_WriteByte(0x16, 0);
cdce913_I2C_WriteByte(0x17, 0);
reg18 = (N >> 4) & 0xFFF;
reg19 = (N & 0xf) << 4 | (R & 0xf0) >> 5;
reg1A = (R & 0x1f) << 3 | ((Q >> 3) & 0x7);
reg1B = (Q & 0x7) << 5 | (P & 0x07) << 2 | (f_range & 0x03);
cdce913_I2C_WriteByte(0x18, reg18);
cdce913_I2C_WriteByte(0x19, reg19);
cdce913_I2C_WriteByte(0x1A, reg1A);
cdce913_I2C_WriteByte(0x1B, reg1B);
cdce913_I2C_WriteByte(0x1C, N);
cdce913_I2C_WriteByte(0x1D, ((N & 0xf) << 4) | (R & 0xf0));
cdce913_I2C_WriteByte(0x1E, (R & 0x0f) | (Q & 0xf0));
cdce913_I2C_WriteByte(0x1F, ((Q & 0x07) << 5) | ((P & 0x07) << 2) | (f_range & 0x03));
}
//void CDCE_Init_set(uint16_t f_out)
//{
// uint8_t read_back;
// uint8_t i = 0;
// uint32_t M, N, Pdiv, Q, R;
// uint8_t reg18, reg19, reg1A, reg1B;
// int P;
// uint16_t f_vco = f_out;
// bool result = false;
// uint8_t f_range;
// while (f_vco < 80)
// {
// i++;
// f_vco = f_out * i;
// }
// while (f_vco < 231)
// {
// for (N = 4095; N > 0; N--)
// {
// for (M = 511; M > 0; M--)
// {
// if ((N * CLK_IN / M) == f_vco)
// {
// {
// result = true;
// break;
// }
// }
// }
// if (result)
// {
// break;
// }
// }
// if (result)
// {
// break;
// }
// else
// {
// i++;
// f_vco = f_out * i;
// }
// }
// P = 4 - (int)((log((double)N / (double)M))/log(2));
// if (P < 0)
// {
// P = 0;
// }
// Q = (int)((double)N * pow(2, (double)P) / (double)M);
// R = (double)N * pow(2, (double)P) - M * Q;
// if (f_vco < 125)
// {
// f_range = 0;
// }
// else if ((f_vco >= 125) && (f_vco < 150))
// {
// f_range = 1;
// }
// else if ((f_vco >= 150) && (f_vco < 175))
// {
// f_range = 2;
// }
// else
// {
// f_range = 3;
// }
// Pdiv = f_vco/ f_out;
// cdce913_I2C_WriteByte(0x02, 0xB4);
// cdce913_I2C_WriteByte(0x03, (uint8_t)Pdiv);
// cdce913_I2C_WriteByte(0x04, 0x02);
// cdce913_I2C_WriteByte(0x05, 0x50);
// cdce913_I2C_WriteByte(0x06, 0x40);
//
// cdce913_I2C_WriteByte(0x12, 0x00);
// cdce913_I2C_WriteByte(0x13, 0x00);
// cdce913_I2C_WriteByte(0x14, 0x6D); //Y2,Y3Ñ¡Ôñ
// cdce913_I2C_WriteByte(0x15, 0x02);
//
// cdce913_I2C_WriteByte(0x16, 0);
// cdce913_I2C_WriteByte(0x17, 0);
// reg18 = (N >> 4) & 0xFFF;
// reg19 = (N & 0xf) << 4 | (R & 0xf0) >> 5;
// reg1A = (R & 0x1f) << 3 | ((Q >> 3) & 0x7);
// reg1B = (Q & 0x7) << 5 | (P & 0x07) << 2 | (f_range & 0x03);
// cdce913_I2C_WriteByte(0x18, reg18);
// cdce913_I2C_WriteByte(0x19, reg19);
// cdce913_I2C_WriteByte(0x1A, reg1A);
// cdce913_I2C_WriteByte(0x1B, reg1B);
// cdce913_I2C_WriteByte(0x1C, N);
// cdce913_I2C_WriteByte(0x1D, ((N & 0xf) << 4) | (R & 0xf0));
// cdce913_I2C_WriteByte(0x1E, (R & 0x0f) | (Q & 0xf0));
// cdce913_I2C_WriteByte(0x1F, ((Q & 0x07) << 5) | ((P & 0x07) << 2) | (f_range & 0x03));
//}
Please help me see what the problem is.
Thanks so much.
Best regards,
Yuki