Part Number: LMX2594
Hi team,
Can LMX2594 work with fMULT=20MHz?
In the datasheet, fMULT range is defined as 30MHz to 70MHz.
My customer confirmed that it works with fMULT=20MHz on the EVM (lock and phase noise are OK).
So they assume it should work with lower frequency like 20MHz.
Verified condition is below:
- fREF :10MHz
- Input doubler : ON
- fMULT :20MHz
- fPFD :100MHz
- fVCO :8000MHz
Regards,
Itoh