Part Number: CDCDB400
Hi
Please recommend one input and two output, or one input and four output clock buffer The following are the requirements of this clock buffer thanks
1. 100MHz input and 100MHz output
2. Output Impedance 85-ohms
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCDB400
Hi
Please recommend one input and two output, or one input and four output clock buffer The following are the requirements of this clock buffer thanks
1. 100MHz input and 100MHz output
2. Output Impedance 85-ohms
Hi Gareth,
The CDCDB400 is a 1 HCSL input, 4 HCSL output buffer with integrated 85 ohm output impedance by default. It can accept 100MHz input/output.
Regards,
Jennifer