Part Number: LMX2694-EP
Hello team,
I want to confirm some point about phase shift description of LMX2694.
Q1)
I want to confirm the definition of "Phase shift in degrees".
Does "Phase shift in degrees" mean the amount of shift in relation to the fVCO?
For example, if fVCO=10GHz is set, would 1 period of 10GHz( = 100ps) corresponds to 360°?
Q2)
In datasheet "Figure 7-5. Determining the SYNC Category", there is a description of "No limitations on fOSC" in diagram of Category2.
Does this "limitation" mean limitation described in "Table 7-13. SYNC Pin Timing Characteristics for Category 3 SYNC"? (fOSC:40MHz(max))
For example, does this mention signals like 155.52MHz could be input for Category2?
Best Regards,
Ryotaro Fukui