Part Number: LMK04828
Dear Technical Support Team,
I'd like to use two LMK04828 and synchronize between output clocks as much as possible.
My idea is to input one oscout (buffered LVDS) into the other clkin0 or clkin1.
Since ADC and DAC compatible with JESD204B are not used, LMK04828 is used as a clock generator, and SYNC and SYSREF are unnecessary.
See attached two tsc files and clock tree(pdf). Could you check the settings of LMK04828?
If you have reference design to synchronize between two LMK04828EVM , could you share it?
LMK04828_OSCin10MHz_ADC_FPGA_2022.01.07.tcs
LMK04828_OSCin10MHz_DAC__2022.01.07.tcs
Best Regards,
ttd