This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: max output frequency with the VCO

Part Number: LMX2595
Other Parts Discussed in Thread: LMX2820

Hi TI experts,

Will it be possible to extend the frequency up to 15250MHz with the VCO only? In the description It is mentionned the max frequency at 15100MHz.

We prefer to avoid if possible the doubler as it creates 1/2 harmonics.

Thanks,

Nicolas