Part Number: LMK05028
Hi
When I see 9.5.5 General Register Programming Sequence in the rev.A datasheet, I have some questions. Please support following three questions.
At fourth sequence, "Write the register settings from lower to higher addresses (R0 to R647) while applying the following register mask (Do not modify mask bits = 1):"
I think R785 is the last register LMK05028 has, why to write until R647?
The word "mask" means the bits with masked as 1 do not be modified, for example, Mask R12 = A5h means R12[7],[5],[2],[0] must not be written, correct?
At sixth sequence, "Write 1b to R12[7]) to begin normal device operation (starting with VCO calibration and PLL start-up)"
[7] is same with fifth, did this want to mention "Write 1b to R12[0]" ?
Best regards,
Hideki