Part Number: LMX2592
Other Parts Discussed in Thread: LMX2594
We have a multiple boards structure where each board has its own PLL (LMX2592). the RefClk is common to all boards but the number of clock buffers for each board is different.
in the example below, you can see that PLL #2 get RefCLK after passing 2 CLK Buffers while for PLL #1, it passes only 1 CLK Buffer.
we are using the PLL in Integer Mode only!

Questions:
1. Given the input phase to the 2 PLLs varies over temperature due to the clock buffer (phase variance changes between the 2 PLL inputs) what will be the phase variation at the output of the 2 PLLs
example: if the PLL RefCLK phase changes (over temperature) by 1Deg (due to changes in the clock buffer), what should be the expected phase changes in the PLL output? is it 1Deg as well or 1Deg times Fout/Fin
2. Given we will swap to the LMX2594 (with the SYNC input), can we overcome this none controled phase difference?