This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03806: LMK03806 can't output Clock in crystal Mode

Part Number: LMK03806


Hi 

In our application,We use LMK03806BISEQ in crystal mode and the lmk03806 clock can't output. The crystal is 20 MHZ.

When we use LMK03806BISEQ in external clock mode, lmk03806 clock can output.

Attached is our schematic and configuration file。 Please help up check it.

Thanks

LMK03806.pdf

R0 (INIT)	0x80020140
R0	0x00000960
R1	0x80000201
R2	0x80000202
R3	0x00000323
R4	0x00000284
R5	0x80000205
R6	0x00010006
R7	0x81000007
R8	0x00100008
R9	0x55555549
R10	0x9002400A
R11	0x3401202B
R12	0x130C006C
R13	0x3B03826D
R14	0x0300000E
R16	0xC1550410
R24	0x00000018
R26	0x8FA4E21A
R28	0x0010001C
R29	0x0080033D
R30	0x0500033E
R31	0x001F001F