Other Parts Discussed in Thread: LMK04832, USB2ANY, LP3878
Hello,
I'm trying to get a clock out of 983.04MHz and have this signal synced to a 10MHz external signal. The setup I am going for is described in the photos below:


I was wondering if you could provide the configuration file and to confirm my hardware setup is correct. On the photo of the hardware the circle next to "1" is the external reference frequency of 122.88MHz (as recommended in user guide, and not shown on my diagram above) coming from my SigGen.
The other circle next to "2" in the hardware photo is the SYNC pin and I am injecting a 10MHz external signal also from my SigGen however I am not able to get the PLL to lock. Any insight would be much apprecaited.
KR,
Alex