Are the inputs to the LMK04832-SP cold-sparing? Particularly the OSC+/- inputs. In other words, if the device is unpowered but the input is being driven, will this stress the device?
I saw another E2E entry asking about cold-sparing on the SPI inputs and the response indicated that the ESD diodes might start conducting resulting in high current draw. I assume this will hold for other input control inoput pins but not sure about clock inputs like OSC+/-.