This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: About R13(INT_LIVE) Register

Part Number: LMK03318
Other Parts Discussed in Thread: LMK03328

Hello Team,

My customer has questions.

The value of register R13 (INT_LIVE) (R13[6]) is always read as "0" regardless of the status (0 or 1) of the STATUS0 pin set to "PRIREF loss of signal" in register R27.

Also, the value of register R13 (INT_LIVE) (R13[6]) is always read as "0" regardless of the status (0 or 1) of the STATUS1 pin set to "LOL" in register R28.

Is there any other procedure that I should do? For example, "There is a latch command and the value needs to be updated" in advance.

Regards,

Masakazu