This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2592: Phase noise performance between a 150MHz and 100MHz reference.

Part Number: LMX2592


Hi team,

if we decrease the reference from 150MHZ to 100MHZ. how does this impact the integrated phase noise performance? which is better?

if OSCin Doubler uses 100MHz reference, will this achieve better phase noise than using 150MHZ reference with no doubler?

Thanks,

Kevin 

  • Hi Kevin,

    As a general rule, decreasing reference frequency tends to mean decreasing the PFD frequency, which increases the N divider used and increases the reference noise multiplication at the output. So, usually a reduction in PFD frequency results in an increase in integrated noise within the loop bandwidth, and a reduction in loop bandwidth overall. Sometimes the reference frequency is independent of the PFD frequency, and there would be no change in this case: assuming you have an equally-good frequency-scaled 100MHz and 150MHz reference, but a PFD frequency of 50MHz, both cases would have identical phase noise performance.

    Usually the 100MHz + OSCin doubler will outperform the 150MHz reference with no doubler, but there are restrictions on the minimum N divider permitted by LMX2592 which make it hard to say definitively that one is always better than the other. For example, the minimum N-divider restriction of 30 with 4th order modulator makes it impossible to use 200MHz PFD frequency below 6GHz VCO. Enabling the doubler in this case would just add to the 1/f noise, and the doubler output would need to be divided again to satisfy the minimum N-divide constraint.

    I strongly encourage you to simulate your desired conditions in PLLatinum Sim, a tool we built specifically to make these comparisons possible for our customers. PLLatinum Sim will warn you graphically if you have prepared an invalid configuration (e.g. violate the minimum N-divider requirement for a certain modulator order), and can calculate the integrated phase noise for any desired configuration.

    Regards,

    Derek Payne