Part Number: LMX2820
Other Parts Discussed in Thread: SN74LV125A,
Trying to run this device with a standard SPI bus interface (beagle bone black) and am unable to approach the rated speed of 40MHz. This is not surprising, since I am going through a harness, but I cannot even reach 4MHz of clock speed before the connection becomes intermittent. I am not the only customer who has this experience, and even so it was with a different SPI bus interface on a different system.
Anecdotally, it was noted that clock edges appeared to be "blunted" by some aspect of the input circuitry, perhaps a parasitic capacitance of a non-linear nature.
If there are errata for this part, with respect to timing or otherwise, then please provide it on the website.
Regards,
Luke