Part Number: CDCDB803
Hey team,
Just a few questions regarding the 1:8 clock buffer!
- What is the common mode for clock input?
- If AC coupled, does it need to be biased?
- Does clock input have internal termination or not?
Thanks for your help,
Cameron
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCDB803
Hey team,
Just a few questions regarding the 1:8 clock buffer!
Thanks for your help,
Cameron
Hello Cameron,
1. The input voltage swing requirements are from 200 mV to 2.3 V
2. No biasing is required as the termination type is LP-HCSL.
3. The only internal termination for the clock inputs is a small input capacitance across the differential pair. The clock inputs are LP-HCSL differential clock inputs and are typically connected directly to the differential output of the clock source.
Regards,
Kia Rahbar
Hey Kia, quick clarification from the customer on the above questions.
"I asked about input bias, but you repeated datasheet AC parameters. Let me explain what I try to find out. Input for CDCDB803 must be AC coupled due to different power domains. Do I need to bias input of the CDCDB803 and to what value if yes?"
Hello Cameron,
There are no issues with AC coupling the input and no biasing is needed.
Regards,
Kia Rahbar