Part Number: LMX2694-EP
Other Parts Discussed in Thread: LMK04828, LMK04832, , LMK1C1102
I have multiple questions. I have an application where I need the extended temperature range and to output a frequency of either approx. 10.5GHz or 14.5GHz. Due to a stability specification I was considering using two parts. The first would be a jitter cleaner part that also has extended temperature range to output 100MHz (or other) to feed to the LMX2694 to output the frequency(s) mentioned above. I would need approx. -109dBc/Hz max. @ 100kHz offset for 14.5GHz or approx. -112dBc/Hz max at 11GHz. I believe the noise floor of the jitter cleaners is affecting this. So, to my questions:
1) Are you in agreement the 100kHz offset of the jitter cleaner parts (LMK04828 or LMK04832) would prevent meeting the 100kHz offset specification (in PLLatinum it shows a -160dBc/Hz floor).
2) Do you have any phase noise plots or data over temperature for the LMX2694EP parts?
3) If the jitter cleaner is indeed affecting the 100kHz offset, do you have any extended range PLL's (OR an output on the LMK series) that doesn't use differential outputs that can supply the reference for the LMX2694.
Thanks!