Part Number: LMX2595
Hi Team,
We are getting o/p power of LMX2595 is about -3 dB@15 GHz but in datasheet, it is 7 dB. i have used inductive pull up of 1 nH as recommended in datasheet. In EVM also max o/p power is about 0 dB. Could you explain this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2595
Hi Team,
We are getting o/p power of LMX2595 is about -3 dB@15 GHz but in datasheet, it is 7 dB. i have used inductive pull up of 1 nH as recommended in datasheet. In EVM also max o/p power is about 0 dB. Could you explain this.
Hi Ajay,
Would you please change the 0.3pF capacitors to a bigger value?
If RFoutB is not using, you can simply leave the output floating.
Hi Noel,
Thanks for suggestion, I have already changed o/p capacitor to 0.01 uF( in place of 0.3 pF. but we are not getting positive o/p such as 1dB or 2 dB. I will leave RFoutB floating and check if there any change in LMX o/p.
Thanks