Part Number: LMK04610
Other Parts Discussed in Thread: LMX2594, , LMK04616, LMK04832
Dear TI Clock and Timing Team,
In our application we are using the LMK04610 as a jitter cleaner to clean a 128 MHz reference frequency, in combination with an external 128 MHz VCXO. The LMK04610 is used in PLL1 only mode to clean the reference frequency using a BW of about 10 Hz. The 128MHz outputs of the LMK04610 then provide the clean reference to separate external synthesizers to produce 4.096 GHz (LMX2594) sampling clocks, and is also divided in the LMK04610 to give SYSREF signals, which feed high speed 4GS/s ADCs. We have multiple of these boards that need to be synchronized.
In our application of multi element phase array receiver it is critical that the phase of multiple boards and the 4 GHz sampling clocks are precisely stable. Given the sample period is about 250 ps we need stability of order 10s of ps at constant temperature, which we do achieve with other typical PLLs in previous designs.
We are seeing, though, that the phase delay between the ref input and the output of the PLL1 jitter cleaner appears to wander randomly on sub Hz time scales, in contrast to what you would expect of a phase locked loop? When multiplied up to 4 GHz this causes large changes in phase between input and output and between multiple boards. On investigating deeper we believe it is the LMK04610 PLL1 itself that appears to have the wander.
On searching the forum today for clues I came across this comment by a TI employee regarding the LMK04610 PLL1.