Part Number: CDCDB400
Hi,
From datasheet, below pin are NC.
What if customer connect these pin to GND, what will happen?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jim,
All these pins can be grounded.
9,10,11,17 are true NC that they don’t go inside the die, so there is no issue with tying them to GND.
Pin 8 is used as SCANMODE_EN so grounding it is not an issue.
Pin 30 is ATP so it is high impedance in mission mode and there is no issue of driving that pin.
Regards,
Kia Rahbar