Part Number: TLC555
Hi,
I designed a circuit to turn ON and OFF an LED using a vibration switch and a 555 timers. I am facing an issue if someone can help me with it.
I want to turn ON NMOS in normal condition and control LED ON/OFF using a vibration switch which works almost. Now when the gate(Dock Signal port/net) of NMOS is connected with GND then I need to turn OFF the LED until the (Switch port/net) is connected with GND.
The issue is when I connected the gate of NMOS with GND and if LED is glowing then it keeps glowing. Can anyone help me to understand why it is like that? I am using NMOS as a switch.
Thanks