Hello Team!
We are utilizing TICS configuration attached below. We are operating in CLKin_Sel_Manual mode and able to obtain a lock on CLKin0 (10MHz) on power on but loose lock 30-60s after startup and are unable to reacquire the signal with holdover disabled. The input is a 10 MHz LVDS fed from an external source. With our configuration, CLKin1 is able to maintain signal lock (different 10 MHz source). To clarify we are loosing DLD on PLL1, PLL2 continues to hold DLD.
Register 0x183 reports 0x09
Register 0x184 reports 0x48
Register 0x185 reports 0xCD
Register 0x188 reports 0x41
Just looking for some insight on our configuration.