Part Number: CDCVF2510
Other Parts Discussed in Thread: CDCE706, CDCE6214
Hi
I am using the CDCVF2510 at Vcc=2.5V to generate a clock to a FPGA
The FPGA requires that this clock will have a Trise of up to 500pS (10%-90%)
Looking at the CDCVF datasheet I see it has at Vcc=2.5V Tr minimum slewrate is 0.5V/nS. This will sum
at a rise from 0.4V to 1.7V to almost 3nS !!
With such Tr , there is no way to reach the promised Fmax of 170Mhz (5.9nS)
Even if I look at best slewrate (1.4V/nS) I am facing Tr of about 1nS, still far from the FPGA required 500pS.
Are my calculations are correct and the CDCVF best Trise at Vcc=2.5V is merely 1nS ?
If so, is there another clock generator (x5 as minimum fanout) that can meet the FPGA requirement?
Any suggestion how to improve my timing will be appreciated
Thanks
Amnon